Other Parts Discussed in Thread: PSPICE-FOR-TI
I would like you to check the circuit.
Input voltage: 5 V, 9 V, 15 V, 20 V
Output voltage: 5V, 9V, 15V, 20V
Output current: 3A (MAX) It is designed according to the circuit diagram of TPS65988EVM.
However, use a ceramic capacitor for the output capacitor. I checked "8.2.2.2 Output Capacitor Selection (COUT)", It says that you have to insert a series resistor, Where and how many Ω resistance values should I put in?