Hi,
I appreciate this is an old part, but I'm looking for clarification on the suggested 'fast transient' network that can be added to the feedback network.
From TPS63020 Datasheet - values are 68kohm and 4.7pF (estimated zero = 33kHz, pole = 150kHz)
From the TPS63020-Q1 datasheet - Values remain the same for the feedforward network, but R1/R2 is much lower affecting zero/pole response
Estimated zero=100k, pole=271kHz
Is there a vast difference in between the two parts or is there an error in documentation? Or something else?
Please can you advise which network is correct?
Thanks, Josh