Hi Expert,
As you know, TPS737-q1 can output 1A. But the use case could be very limited. As an example, I want 5Vto3.3V @1A. The power dissipated on TPS737-q1 is about 1.7W. The junction temp could be 88℃. If we think ambient temp is 85℃, it exceeds the range. I just don't know exactly under what situation it can be used since I think 1.7V voltage drop is small enough. Thanks!
BR,
Elec Cheng