This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS717: TPS71733DCKR: P-P replacement

Part Number: TPS717
Other Parts Discussed in Thread: TLV700, LP5951

Hi Sir,

due to TPS71733DCKR constraint supply by the LBC7, could you pls kindly suggest the P-P device?

one more spec request is that the VIN needs to > 6.5V. 

Thanks a lot!

BR, 

Sean Liao

  • Sean,

    The only p2p parts are 

    TLV70033DCKR and LP5951MG-3.3/NOPB. Unfortunately, they also don't have inventory.

      TPS717 TLV700 LP5951
    AEC Q100 NO NO NO
    Output Options Adjustable Output, Fixed Output Fixed Output Fixed Output
    Iout (Max) (A) 0.15 0.2 0.15
    Vin (Max) (V) 6.5 5.5 5.5
    Vin (Min) (V) 2.5 2 1.8
    Vout (Max) (V) 5 3.6 3.7
    Vout (Min) (V) 0.9 1.2 1.3
    Fixed Output Options (V) 0.9, 1, 1.1, 1.2, 1.3, 1.5, 1.8, 1.85, 1.9, 2.1, 2.5, 2.6, 2.7, 2.8, 2.85, 2.9, 3, 3.3, 4.5, 5 1.2, 1.3, 1.5, 1.8, 1.9, 2.2, 2.5, 2.8, 2.9, 3, 3.1, 3.2, 3.3, 3.6 1.3, 1.5, 1.8, 2, 2.5, 2.8, 3, 3.3, 3.7
    Enable YES YES YES
    Power Good NO NO NO
    Output Capacitor Type Ceramic Ceramic Ceramic
    PSRR @ 100KHz (dB) 67 51 32
    Noise (uVrms) 30 48 125
    Accuracy (%) 3 2.5 3
    Vdo (Typ) (mV) 170 175 200
    Iq (Typ) (mA) 0.045 0.03 0.029
    Thermal Resistance θJA (°C/W) 71 236 196
    Min Package Area (mm2) 2.25 2.25 4.2
    Package Type SC70, WSON, WSON SC70, SOT-23-THIN, WSON

    SC70, SOT-23

    Regards,

    Prakash L