Hello
I am using the BQ25887 on the balancer 5 click board (PID: MIKROE-3853) and I have a question regarding the ADC control register (REG15 register). I read the subsection 8.3.5 (Integrated 16-Bit ADC for Monitoring) and I have tried to configure REG15 and enable the ADC with the ADC_EN bit. Afterwards I checked if setting the register was successful but found out that the reset value which is 0x30 is still there. I have already checked if the conditions
VVBAT > VBAT_UVLO_RISING or VBUS > VBUS_UVLO_RISING
are met and this is true for either setting. I have already checked the I2C signal and if the transmission is correct. Can you tell me what else I can check or what I might have overlooked since I can't manage to fix this problem.
Best regards,
Markus