This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSD86360Q5D: Design feasibility

Part Number: CSD86360Q5D
Other Parts Discussed in Thread: TPS53015, TPS51916, TPS51215A, CSD87335Q3D, CSD87384M, CSD87588N, CSD87352Q5D

Hi sir,

Can I use FET (CSD86360Q5D),  in the following design,

is there any issue?

Design[1]

Use IC: tps53015

VIN 5V Vout 3.3V IOUT Max 10A

Design[2]

Use IC: tps51916

VIN 5V Vout 1.2V (DDR4 VDDQ) IOUT Max 10A

Design[3]

Use IC: tps51215a

VIN 5V Vout 1.8V IOUT Max 15A

Thanks.