Other Parts Discussed in Thread: TPS53015, TPS51916, TPS51215A, CSD87335Q3D, CSD87384M, CSD87588N, CSD87352Q5D
Hi sir,
Can I use FET (CSD86360Q5D), in the following design,
is there any issue?
Design[1]
Use IC: tps53015
VIN 5V Vout 3.3V IOUT Max 10A
Design[2]
Use IC: tps51916
VIN 5V Vout 1.2V (DDR4 VDDQ) IOUT Max 10A
Design[3]
Use IC: tps51215a
VIN 5V Vout 1.8V IOUT Max 15A
Thanks.