This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24195: BQ24195 warming up when powered only by the battery.

Part Number: BQ24195

With the system powered only by the battery, without an external source, the current on the BAT pin is 160 mA. The IC is heating up. This current should have a value close to 15mA, right? What could be happening? This is my schemattic for reference. R12, R13, R14, R15, R4, R3 are not fitted. I'm not using the I2C.