Other Parts Discussed in Thread: TPS92200
Dear TI team,
could you check converter can output voltage below condition ?
I'm worried about max on duty ratio. it is almost 100%
(1) Vin : 5V
(2) Vout : 4.6V , 0.6A
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
TPS54200 can't meet such high convert ratio. Please consider TPS92200 and its maximum duty cycle can reach 99%.
Robin
Dear robin,
What is the max duty cycle of TPS54200 ? I can't find it in datasheet
Best regards,
Hi,
The typical switching frequency is 600kHz while the typical minimum on-time is 90ns, so the typical minimum duty cycle is about 90ns/600kHz=94%.
Robin