This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5860: Some LEDs doesn't light up

Part Number: LP5860
Other Parts Discussed in Thread: USB2ANY,

Hi Team,

Our customer built an LP5860 prototype board using the SPI Interface. He wants to test the prototype board so I told him to connect the SPI port of USB2ANY development tool to the corresponding SPI port of LP5860. I also told him to connect the IFS pin of the LP5860 to VCC. When he ran the LP586x GUI only 66 of the 198 LEDs lit up as shown in the picture below. Please see attached matrix and schematic diagram. 

   1500-AMZ-0001-00_REV-01_LED.pdf

Is the GUI capable of lighting up all LED in this setup? What could be the cause of the other LEDs not lighting up?

Regards,

Danilo