Part Number: UCC27321
I am using a Ucc27321 gate drive to control IPB120P04P4L-03 mosfet @ 12volts driving resistive load.
Issue is when testing device for short circuit control I get a large voltage spike across mosfet Source of about ~30 volts with about 30us duration. The Source is tied to 12volt VCC that also powers UCC27321. This causes UCC27311 to exceed Max voltage of 15V and therefore destroys UCC27321.
Short circuit test is conducted by tying Mosfet R Output to ground. Processor turns Gate drive is turned on the senses current from AD8218 and turns gate back off within a 1ms. Turn off causes pulse.
PCB is 4 layer with ground plane.
I have transient voltage suppressor SMBJ15A (15Volt) across VCC near UCC27321 , but it does nothing to keep spike below 15 volts.
How can I protect UCC device?
t