Hello E2E,
Regards,
Carlo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello E2E,
Based on Figure 29, the LM2831Z has a 3MHz switching frequency but the inductor suggested only supports up to 100kHz, will this work?
Also, for inductor selection, please share the formula for this:
1. inductor value
2. frequency
3. Isat greater than the load current
Thank you for the help.
Regards,
Carlo
Hi Carlo,
If we refer to the datasheet of the recommended inductor, the inductance vs frequency graph shows that the inductance remains nearly constant at 1.6uH up to 90MHz approximately. Please see the screenshot attached below.
You can use the formula below for calculating the value of the inductor. I would recommend to look into this app note for more details about it.
Let me know if you have further questions on this.
Thank you!
Best regards
Sneha
Hi Carlo,
Do you have further questions related to this thread? If there are no more questions, please close the thread by hitting the "Resolved" icon.
Thank you!
Best regards
Sneha