Other Parts Discussed in Thread: TPS92641
hi,
from TPS92641 EVM below,
https://www.ti.com/lit/pdf/slvu823
we get the setting below.
Vin= 43 - 53V
Vturn_on=40.5V
Vhys = 15.5V
Vovp=48.9V
VLED=40V
Question 1:
Vturn_off(40.5-15.5)=25V
Vin must lower than 25V to turn off tps92641, but the VLED is 40V. Why does EVM set this value?
question 2:
Vin,max is 53V but Vovp is 48.9V. Is the setting too close to Vin,max and it may never trigger OVP?
BR,
frank