Other Parts Discussed in Thread: LM5158, LM2621
Hello,
I would like to know if the LMR62014 will be appropriate for my application.
Output Voltage: 14V/15V
Input Voltage Range: 5.5V - 12V (actual range is 6V-12V, but 5.5 is the worst case scenario)
Load Current: 400mA
My initial computation showed it near 500mA max load current and the figure 22 in the datasheet might suggest it would be between 400-600mA? Is this accurate?
Will 400mA be too close to the absolute maximum load current for these set of parameters?
On Another Note: If my load current is doubled to 800mA. What alternative part to the LMR62014 would be recommended?
Thanks,
Deniel