Other Parts Discussed in Thread: CSD16301Q2
Hello,
I'm using the TPS81256 to supply power to a laser diode module. I'm modulating the laser by using a CSD16301Q2 MOSFET on the low side of the module to modulate the connection to ground - traditional LED type driver. The laser module has an impedance of ~312 ohms. I cannot measure the capacitance of the module - measures basically 0 pF. From the scope trace, I see the device is turning off fast, likely due to the internal 312 ohms, but charging the module/capacitor is very slow causing the output signal to never attain the 5VDC supplied by the TPS81256. Any suggestions as to how I can make this module turn on quicker?
Thanks,
Patrick