Hello,
I have the question about the regulator TPS76333. I found in the pdf such information:
"The TPS763xx pass element has a built-in back diode that safely conducts reverse currents when the input
voltage drops below the output voltage (e.g., during power down). Current is conducted from the output to the
input and is not internally limited. If extended reverse voltage is anticipated, external limiting might be
appropriate."
I have the question, what is the maximum reverse current that can flow through back diode ??
Regards
Michal