Other Parts Discussed in Thread: LMR33620
Hello,
A customer of mine is working on the LMR36015,
The maximum current they will want to use is 300mA, Once load current is low as 150mA they are seeing a decrease in the frequency – see attached measurements:
They see the following frequencies at 24V nominal input:
Load |
Frequency |
0mA |
8.6Khz |
150mA |
770Khz |
300mA |
830Khz |
410mA & Above |
1Mhz |
The output does stays at 11V.
Can you please advise if this is valid?
From my check the cause is because the Minimum Switch On-Time is reached – can you confirm?