I have a design where the Vin pin of the tps61042 is connected directly to a battery and the ctrl pin is connected to a microcontroller that runs off a 3.3 V supply. It's possible for the ctrl pin to be at 3.3 V when the Vin pin is at 2.5 V or less under low battery conditions. I've had three chips fail, all when the battery was low.