Hello,
I am observing an output current repeatability error, only on a few units (around 2%) on a production, using Vadj to control the output current.
The production test I am doing is setting Vadj from 0 to 1V which give 650 mA output current +/- 50 mA depending on board. Usually output current is consistent all the time on a SAME BOARD within 1 mA.
Sometimes, on a few units gives either for instance 650 mA or 620 mA. There seems to have only two scenarios possible 650 or 620 mA for the SAME BOARD. Settting Vadj to to 0v and back to 1V will switch to 650 or 620 randomly.
- I checked Vadj which is exactly the same with no ripple in both scenario
- Vin is the same in both scenario
- Load is the same in both scenario
- Switching frequency is a little bit different
Am I clear enough in my explanations ?
Any idea where to look at ?
Thanks !