Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2937: 3.3V

Part Number: LM2937

Hi,

Good Day. I have a customer who is working with LM2937ET-3.3/NOPB. Please see below his query for your reference. Thank you very much.

I'm looking at the datasheet for the LM2937ET-3.3 (LM2937ET-3.3/NOPB) and I've noticed section 6 appears to be missing information on the 3.3 version of this product family. I see specifications for the 5V, 8V, 10V, 12V and 15V versions, but nothing for the 3.3V. While I don't think most of this information will be especially critical to our specific use case, I thought it would be important to share this discrepancy.

I would like to confirm the min and max output voltage of this device however.

Best Regards,

Ray Vincent