Other Parts Discussed in Thread: BQ24079T,
Hi team,
My customer considers to use BQ25170 and he is asking about STAT pin behavior.
Datasheet states that STAT pin behaves as below.
1.) Charge in progress -- Low
2.) Charge complete -- High
3.) Fault -- Blink at 1Hz rate
Meanwhile, STAT pin of Fig 8-3(power-up without battery) blinks around 120ms which is faster than 1Hz.
In addition to above 3 status, STAT pin blinks 120ms frequency when there is no battery. Is this understanding correct?
Also, could you please provide equation to determine RP and RS of TS which can calculate arbitrary threshold?
Best regards,
Shota Mago
Regards,
Shota Mago