Other Parts Discussed in Thread: UCC28180, UCC256402, TIDA-01494
Hello community,
I need your help in designing a switching power supply. I got a schematic and BOM from Designing the transformer to match the circuit from WEBENCH® POWER DESIGNER but I have a question how to wind the transformer.
I have made the following settings:
Input:
Supply type: AC
Frequency: 50Hz
Voltage 120V-230V
Output:
48V DC 12A normally 10A
Max Ambient Temp:55°C
It spit out a circuit around the UCC28600DR. So far so good. Even the availability looks good, which is a miracle nowadays.
However, there is virtually no information about the transformer:
Ns1toNp: 758.26 m Ns2toNp: 247.07 m Lp: 20.82 µH
It is written in the Bom.
Do any of you have experience with a similar circuit? And maybe has a core he can recommend and a winding ratio?
Or is there even a transformer with suitable properties already wound?
I would be overjoyed about any help!
Best regards!
Roger