This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61178: High current at no load (yet another)

Part Number: TPS61178

Hello, I have created 5->11V boost converter using TPS61178. I used this chip previously w/o any problem. This is what I got:

EN=HiZ: no input current at all (few mAmps) - doesn't matter on load (strange, isn't ? Slight smile)

EN=3.3V: 160mA - no load condition

EN=3.3V: 5150mA with Iz=1.52A (Rz=high power wire wound resistor)

I have attached schematics, PCB and scope plot for 0mA and 1.5A (blue=DC output,red=AC output). Power source - 30V/10A low noise non-switched power supply (Vout=5.0V)

PCB details: 6 layers, under TOP layer is solid ground. Nothing special.

Voltage/ripple seems to be OK (except some ringing ?). L8 is physically depopulated. Input voltage physically delivered to solid VCCUSB top solid.

Any idea what could be wrong ? Thank you !

L.