Other Parts Discussed in Thread: BQ24600, BQ2057, LM3409, BQ25730
TI engineer:
I want to choose an IC or solution that is suitable for current-limiting adapters(example:16.8V 6A),Current-limiting power adapter(16.8v for 4s cell) charging,the power supply is directly connected to the battery, charging to a certain voltage is to adjust the charging current。
I tried the BQ24600, but the efficiency is not too high and the heat is serious, and there is a voltage difference between the input and the output to work normally. It feels unsuitable
I found bq2057, it feels the function is suitable, but unfortunately it does not support 4 strings of batteries ,Then I thought of using constant current IC LM3409,I don't know if it supports 100 duty cycle and whether it can achieve the function I need.


Is there a suitable solution or IC?