Hello,
I have created a charger circuit For 3Cell Li ion Battery BUT After reaching the Battery Voltage 12.22V the battery is not charging but the STAT1 and STAT2 LED'S status are as below
Vin =16V
At Output Pin with Load(Battery) the output Voltage =12V94
Output Current is about 100mA
STAT1 LED is glowing and after few min it start Blinking for (7 Times) and again glow continuously
STAT2 LED is OFF
I am using 0.1 ohm resistor as my Current sense resistor
R ISET1= 10K
R ISET2= 10K
Feedback VOLTAGE DIVIDER resistors are 510k and 100K
Please help me know how I can achieve12V6 and after reaching the Battery Level 12V6 the STAT2 LED should glow