Other Parts Discussed in Thread: LM317
Can you stacking regulators to increase voltage (2 12V to create a 12V and 24V output for example) or can you raise the output level of the 12v using external resistors and which configuration is most stable. The current availability and lead times on parts if forcing me to consider solutions that I would not have done in the past. The 12 V SOT-23 TLV760 is available for now. Thanks Ernie