Hello, when we hot-plug a 24V power adapter to the input of this part, it will fail and measure short thereafter. If we connect the same power adapter cold (make the connection then power the adapter), the system works fine. We did scope the power adapter output and we are measuring a clean 24V ramp with no noticeable overshoot. However, the dv/dt of the rampl when it is hot-plugged is much higher than the adapter powerup dv/dt. We think this high dv/dt may be causing a high inrush current internally and damaging the board. Can you please comment? Thank you.