Hi TI experts,
When I use Pin20 as PDSG, I found that after it is turned on, it is a high-level drive output, and the low level is active. Can I use the Pin20 to directly connect the G pole of the PFET for control? As shown in Figure 1.
In addition, after I turned on Pin20 as PDSG, I found that the power consumption of the protection board increased by 4 times (350uA increased to 1.5mA, as shown in Figure 2, Figure 3). After my analysis, I found that the increase in power consumption was caused by BQ40Z80 turning on Pin20 as PDSG function. Yes, is this normal?
1. If it is normal, the power consumption is too high. Is there any other way to reduce the power consumption?
2. Is it the reason for Pin20 to do high voltage drive output? Then if I change Pin16 as PDSG, will the power consumption be normal?