Hi support team,
There is an inrush current of 9.2A on the output side at startup.
The calculation of the peak current and valley current of the inductor is as follows.
Peak current : 10.2A
Valley current : 8.2A
The peak current is less than 10.5A of "MIN" of "High-side switch current limit threshold".
The valley current is less than 9.5A of "MIN" of "Low-side switch sourcing current limit".
If both of these are met, will the current limit not be activated?
Regards,
Dice-K