Other Parts Discussed in Thread: GPCCEDV, BQ78350, BQSTUDIO
Hi team,
Here's an issue from the customer may need your help:
The description in the reprort of GPCCEDV file is as follows:
CEDV parameters resulting from the fit. If EDVV bit is set to 1, EMF and EDVR0 have to be multiplied by the number of serial cells when written to data flash.
EMF 3517
EDVC0 623
EDVC1 0
EDVR1 89
EDVR0 1375
EDVT0 5229
EDVTC 11
1. Regarding EDVV bit, it cannot be found in Battery Management Studio (bqstudio).Which status bit is referred to in the BQStudio software? Also not found in bq78350 file.
2. Also, "EMF and EDVR0 have to be multiplied by the number of serial cells when written to data flash", dose this mean the current report going to be converted as well? (This report is currently 2 strings of 1 data). If they want to change to 6 string 2, is the following parameter correct?
EMF 10551 (3517/2*6=10551)
EDVC0 623
EDVC1 0
EDVR1 89
EDVR0 4125 (1375*6/2=4125)
EDVT0 5229
EDVTC 11
Could you help check this case? Thanks.
Best Regards,
Cherry