Hello team,
I have a question about bandwidth-limiting resistor described in Datasheet 8.2.2.6.1.
It is explained that implementing this could avoid noise coupling into the control loop, and it is also implemented in the EVM. Though it was not listed in the 8.2 Figure 8. Typical Application schematic.
There were several cases in the E2E forum that circuit without this resister caused output instability. How should I think about conditions that require this resistance and the appropriate resistor values?
Also, when testing with a circuit without limiting resistor (same circuit as Figure 8), the output power was stable when the power consumption was low, so would it be related to power consumption?
Best Regards,
Ryotaro Fukui