Other Parts Discussed in Thread: TPS81256, BQ24075, TPS61027, TPS61022
Hello,
The input of the TPS81256-EVM is provided by a BQ24070X-EVM. When powered from either the battery or USB, the output of the TPS81256 is 5.0V as expected. The TPS81256 will drive a laser diode whos performance (low optical noise) is important to the proper function or our instrument. We're concerned about the electrical noise on the output of the TPS81256 shown in a DC couple state (fig 1) and AC coupled state (fig 2). Do you have suggestions to improve the output noise performance of the TPS81256?
Fig 1
fig 2