Hi,
We want to use LP3879SD-1.2/NOPB, input is 3.3v, output is 1.2v and the load required is aroung 230mA. In the data sheet it is mentioned about the input and output capacitance values(such as min 4.7uF for input and 10uF for output). What voltage rating and tolerance, do we need to select for our application.
Thanks--
Sayyad.