Other Parts Discussed in Thread: SN74AUP2G80,
Hello,
I am using theTLV62569 IC in a buck converter circuit and it uses an Logic EN pin to enable/disable the IC output. Pin high=enabled and Pin Low=disabled. I will have a switch that when closed will connect EN to ground sending it low. Is there any way to use a momentary tactile switch to manage that control. I have seen circuits using a SN74AUP2G80 that would I am sure work but for a simple logic connection that is Hi/Low that seems to be way overkill so I am hoping someone may have a suggestion for some simple solution. Certainly I am not clever enough to work one out:-(
BTW I am hoping to use a Tactile switch as they are very small and all the small ON/OFF switches I have found are too big for my project so I am hoping to use something similar to this https://docs.rs-online.com/4f6e/0900766b810d5f0c.pdf. The current through the switch when EN is connected to Ground will be approx 0.001mA and 3.7v.
Hope someone can advise some ideas so I can explore options.
Regards