This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62912: TI solution suggestion

Part Number: TPS62912


Dear Team,

Do we have any solution can meet these spec as below?

Vin: 12V

Vout: 5V

SW feq: 1.5M (Min)

have FPWM mode.

Eff: 80% (min) from 10mA to 350mA

Many Thanks,

Jimmy

  • Jimmy,

    The TPS62912 is close, as it is FPWM, and switches at 2.2MHz for the 12Vin to 5Vout case.  However the efficiency at 10mA will be below 80% due to the higher Iq of the device and the FPWM.  What is the use case for the device, and can this requirement be adjusted?