Other Parts Discussed in Thread: TPS61029-Q1
Hi,
We are using TPS61240-Q1 in our design with input supply as 3.0V. In the updated design we have added additional load and the total load of 5V0 is 281 mA. I would like to know if the subject device supports this load current at operating temperature of 105 degree Celsius.
From Fig. 5 of the datasheet, I could infer that 300 mA of current is supported by the device when Vin = 3.0 V. Can you please confirm this at operating temperature of 105 °C and let us know if it is 'safe' to use at this environment.
Regards,
Dixit Jones Zachariah