Hi TI,
To avoid drops/noise at measured contacts, caused by BQs current and noise, we use different contacts for BAT (instead of C14) and GNDs (instead of C0) in our application with BQ79614-Q1. In our application there is an high probability of contacting VCx/CBx and GNDs before the BAT pin contacts during hot-plug of the board (with stacked BQs) to the battery modules, that could happen even if there wasn't any stack. I'm afraid that it can damage the internal protection due to current flow from VCx/CBx to internal power rails (don't know which power rail it is) where the "protection diodes" points to. We use the suggested resistor: 100R at VCx pins and 10-30R at CBx pins. We also use the decoupling caps suggested in the design recommendations so we don't have large capacitance at the power pins. We'll also place a 470n from CB14 to BAT, as suggested.
Is this a real issue or TI already covered those hot-plug events with design recommendations?
We thought to isolate GNDs from negative voltage of the module with a MOS and a parallel precharge resistor to power up the BQ and then the BQ will power up the MOS with an BQs output voltage rail. Is that really necessary?
Are there any other possible damage due to hot-plug events and do you have any other recommendation, maybe even with external protecting circuits ?
Thank you very much!
Fatjon