Other Parts Discussed in Thread: CSD18513Q5A
There is a request for a schematic review from a customer.
- The input reverse polarity protection circuit is configured by applying LM74610-Q1. (Case 1.)
- Use 2 motor drivers (DRV8244S-Q1) (input: 4.5 ~ 40Vdc, current peak: 21A)
[Schematic attached]
Q1) Is there any part to be corrected in the circuit diagram? Please review.
Q2) Instead of configuring the CAP at the input terminal at once, I added the CAP to the driver input terminal (C247, C248), is there any problem? If there is a problem, please suggest an alternative solution.
Please check. Thank you.