Hi team,
From the functional block diagram, INH of LMZ31520 has internal pull-up and down resistors.
I recognize they will pull-up the INH pin to VIN * 0.4.
In my customer's system, VIN=5V.
My customer would like to pull-up INH pin more strongly because the INH pin is connected to PG of prior converter, and the PG voltage is externally monitored with 4.4V threshold.
So I'd like to pull-up the INH to >4.4V to set pull-up voltage above the threshold.
For this reason, is it allowed to connect external 1kOhm pull-up resistor to INH pin?
Regards,
Itoh