This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24250: LDO is partially enabled without input voltage

Part Number: BQ24250

Hello,

I am using the BQ24250 ic as charger for a 1 Lithium cell battery. The problem is that the voltage in LDO pin is about 2.15V instead of 0V when no input is connected (5V rail come from a USB connector). It causes power consumption since a couple of resistors is connected to TS pin and GND. 

Do you have any ideas?

Thank you in advance

Here you can find the schematic.