Other Parts Discussed in Thread: TPS548D21
We have an existing design using TPS548D22 with pin 37 connected to gnd via a 1000pF cap.
This is a mature design and seems to have no issues, though I see from some of the posts
that pin 37 should be NC.
Due to supply constraints, can we replace TPS548D22 part with TPS548D21 part, all
else being the same ? Pin 37 is connected 'ONLY' to gnd via 1000pF cap (and to nothing else).
The mode pin has a pullup resistor 100k 1% to pin 31 (BP) and a pulldown resistor of 42.7k 1% to gnd.