Hello,
One of my customers, is using the UCC29002 load share controller. They have an application that uses this chip powered off of a 12V bias to load share for a 15V output, with the sense line essentially right on the adjust pin. The datasheet specifies that this pin should not go above the Vdd but the block diagram shows the ADJ pin being open collector and from this simplified diagram they don’t see an issue. Could you give any detail on this and whether or not having this setup will cause issues or possibly be a reliability concern?
Thanks,
Adam