Hi Team,
just want to check if there is below boost solution.
Vin=4.5V
Vout=50V
Iout = 1A
Q100
Checked website, seems only controller such as LM5122-Q1 can achieve that since Ipeak is very high, right?
Then for converter, such as LM5158-Q1, what's the max Vout it can achieve when Vin=4.5V, Iout=1A? Thanks.
BRs
Given