This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV62568A: When changing from TLV62568

Part Number: TLV62568A
Other Parts Discussed in Thread: TLV62568

Hi team,

I am considering changing from TLV62568 to TLV62568A.
The recommended filter values are different,
 TLV62568 2.2uH, 10uF
 TLV62568A 1.0uH, 22uF
Is there any problem if I use it without changing the filter value?

Best Regards,

  • Hello.

    If I understood right, now you want to use TLV62568A with  2.2uH inductor + 10uF. It is not recommended because TLV62568A is designed and tested/validated with only 1uH inductor. So it can affect the AC response of a device if you use the filter values out of LC table given in the datasheet of the respective device.

    Thanks and Best Regards,

    Farheen