This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH-POWER-DESIGNER: How to change the external FET from a single FET to dual FET in parallel?

Part Number: WEBENCH-POWER-DESIGNER
Other Parts Discussed in Thread: TPS51916

Webench support team,

I can't get a simulation result due to the specification limitation of the external FET used in Webench-Power-Designer. The below is an error message.

How can I change the FET configuration from a single FET to Dual FET in parallel?

My simulation device is TPS51916. The simulation condition is follows.

  • Input Voltage = 9V - 18V
  • Output Voltage = 1.1V
  • Output Current = 20A
  • Ta=30degC