This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM317-N: Input capacitor

Part Number: LM317-N


Hi support team,
In the Typical Application item on the first page of the data sheet,
About C1 (input capacitor).

* Needed if device is more than 6 inches from filter capacitors.

Should I place the C1 if the current is small (eg 30mA) but this distance is longer than 6 inches (eg 12 inches)?

Regards,
Dice-K

  • Hello Dice,

                      We recommend that an input capacitor (C1) be added if the device input pin is located more than 6 inches away from the power supply source. This will compensate for source voltage impedances and improve line transient performance. Thanks!

    Regards,

    Srikanth