Part Number: BQ2022AEVM-001
Other Parts Discussed in Thread: EV2400, BQ2022A
I understand this is the same issue as from other posts, but I could not find a definite resolution to the problem.
The EV2400, with either firmware version 0.28 or 0.32, does not generate the pulse to enable the necessary 12-V level for programming the bq2022 EPROM.
I have tried with two bq2022A EVM's and two EV2400 interfaces. I am able to read data from the device, but none of the write commands work. The power supply is connected, jumper J3 is in place. However, despite whether the setup has an issue or not, an observation at the HDQ connector with either oscilloscope or logic analyzer indicate the EV2400 does not generate the programming pulse. From other posts, I believe firmware version 0.28 should have taken care of this issue, but both customer and I could not make it work.
Do you have suggestions on how to go about this issue?
Thank you!