Other Parts Discussed in Thread: TPS3703,
Hello, I have a question regarding this device and how it works.
Reading the dataseet, I see that the RESET is asserted when the SENSE is below Vit-, and it's released when it's a 5% greater (this is the hysteresis threshold tolerance) So the release of the RESET will be when Vit- + (Vit- * 0,05), is that right?
But what about if I want monitor a voltage with a 2% tolerance, for example.
If I want monitor a 1V with 2% tolerance, the RESET will assert at 0,98V but it won't release until 0,98+(0,98*0,05)=1,029V, that is higher than the nominal voltage, for example, so It might happen that RESET never release if the input voltage does not pass the nominal voltage by 2-3% aprox. In this case, I guess I should choose a supervisor with a lower hysteresis tolerance, right? maybe 1% to monitor voltages with a low tolerance, right?
Thanks!!