Please suggest if AIN pin is not used in UCC21750-Q1 then what will do the AIN pin .If the pin left open or tied to Vcc or GND.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please suggest if AIN pin is not used in UCC21750-Q1 then what will do the AIN pin .If the pin left open or tied to Vcc or GND.
if the APWM system is unused:
1) AIN should be tied to the COM pin (this is connected to IGBT emitter or FET source. If using resistor, use 0ohm.
2) APWM output MUST be left open/floating. tying this pin to GND or VCC will damage the IC.
Please see table below for what to do with unused pins as a reference.
If this answers your question please let me know by pressing the green button.
Best
DImitri