This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90910: Can't Store RAM to Flash

Part Number: UCD90910

I am trying to update a board with UCD90910 on it that was previously programmed, but when I open it in the Fusion Digital Power Designer GUI, it says there is no profile on it and opens with a new one.  When I click "Store RAM to Flash" after importing a saved fan profile (which is successfully being used on others of the same board), an error comes up that says "STORE_DEFAULT sent and ACK.  However, the STORE_DEFAULT_ALL_ERROR bit is set in MFR_STATUS.  Device might be busy writing log to FLASH." as seen in the first picture below.

I looked at the status window, cleared all the faults and logged faults, and tried to store RAM to flash again, but the same message came up.  STORE_DEFAULT_ALL Error comes up before clearing the faults, but a few other faults never clear including MFR, CML, More faults in high byte, and Hardcoded Parms.  These are in the second picture below.  Is there a way to completely reset or wipe the UCD90910 chip so the RAM can be stored to flash again?  Or is there a way to clear the Hardcoded Parms and MFR faults?